AXIS#.HOME.MODE

Description

AXIS#.HOME.MODE specifies the homing procedure of the drive. The homing modes available in the drive are summarized in the following table.

Mode Description

0

Current position

1

Find limit switch

2

Find limit switch then find zero angle

4

Find home switch

5

Find home switch then find zero angle

7

Find zero angle

8

Find end stop

9

Find end stop then find zero angle

12

Find home switch, including end stop detection

13 Absolute Mode - Use Feedback Position
14 Reserved
15 Find next feedback zero position
16 Find home switch using dual edges

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0-2, 4-5, 7-9, 12-16, 19

Default Value

0

Data Type

Integer

See Also

AXIS#.HOME.MOVE

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.HOME.MODE

5008h

02h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6107

1

6107 (0x17db)

AXIS1.HOME.MODE

Unsigned16

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.HOME.MODE

6107

Unsigned16

Read/Write

-

Related Topics

Homing